AXIS#.IL.FOLDFTHRESH

Description

AXIS#.IL.FOLDFTHRESH is the fault level of the current foldback algorithm. If AXIS#.IL.IFOLD drops below the value for AXIS#.IL.FOLDFTHRESH, then a fault is generated and the drive is disabled.

To avoid reaching the current foldback fault level, set AXIS#.IL.FOLDFTHRESHU well below the continuous current value for both the drive and the motor or set the AXIS#.IL.FOLDFTHRESHU value to zero.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Arms

Range

0 to 500 Arms

Default Value

Drive peak current (IPEAK)

Data Type

Float
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
AXIS1.IL.FOLDFTHRESH

500ah

08h

Signed32

-

1000:1

Read only

No

AXIS2.IL.FOLDFTHRESH

510ah

08h

Signed32

-

1000:1

Read only

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.IL.FOLDFTHRESH

5805

16AD

Signed32

Read Only

-

AXIS2.IL.FOLDFTHRESH

71341

116A

Signed32

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.IL.FOLDFTHRESH

5805

Float

Read Only

-